2023-12-14 8:30 AM
I call the following function:
neai_classification(input_user_buffer, output_class_buffer, &id_class);
When the program runs this function, it enters the following function:
void HardFault_Handler(void)
This is the first time to use, if you need other information to help determine the fault location please leave a message, thank you very much
The software used is as follows:
STM32CubeIDE 1.14.0
NanoEdgeAIstudio 4.3.0
The following hardware is used:
NUCLEO-STM32F746ZGT6
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.