2024-01-22 12:02 PM
Hy guys, I want to be able to create a named file in an SD card based on how many files I have in the directory, per example: if I have only 1 file "file1", I'll create the next one as "file2".
I searched the ff.h library, but didn't find anything that seemed usefull. Has anyone know any ideas I might implement to make it work?
Also alternatively, is there a function that reads or compares the name of the file and then create another file with a different name?
Solved! Go to Solution.
2024-02-02 12:20 PM
IT WORKED,
I added a line to break:
2024-01-22 12:18 PM
Hi,
Just read the filenames (++ a counter) until end of dir , then you know how many files in this dir .
(I tested : f_readdir needs about 0,5..1ms , so for 30 files need about 30ms .)
Then make a string with "fileX" (X = ++counter) and open file with this new name, thats it.
.
2024-01-22 12:29 PM
FatFs is designed to be small, there's not specific function to count files, not that I recall one in STDIO or WIN32 either..
Enumerate files via f_opendir() / f_readdir(), filter out directories, and perhaps count FILExxxx.TXT files, or search for largest used case, and increment to the next.
http://elm-chan.org/fsw/ff/doc/readdir.html
2024-02-02 9:44 AM
Hi @AScha.3
I've writed the code to do it, it creates a file"0", even tho there already have a file in the SD. But it doesn't create another one, it keeps updating the file0. Here's the code:
2024-02-02 10:01 AM
Does it count files?
What error does f_open() return?
I cited specific code showing how to count files / directories on a specific path.
It's not hard to corrupt the file system if writing fails or if you lose power, etc.
2024-02-02 10:12 AM - edited 2024-02-02 10:35 AM
Actually no, it isn't entering in the if loop.
The res_dir return FR_INVALID_OBJECT.
I added this:
res = f_opendir(&dir, path);
if(res==FR_OK)
{
res_dir = f_readdir(&dir, &filinfo);
if((res_dir==FR_OK)&&(filinfo.fname[0]!= 0))
{
file_number++;
}
}
And now res is returning FR_INVALID_DRIVE
2024-02-02 11:00 AM
Solved the issue on the errors by putting: res = f_opendir(&dir, "/");
It created a file1 (it already had file0), but it continues not counting after that, it only updates file1
2024-02-02 11:35 AM
Right, because you don't loop.
The cited example uses for (;;) it could use a while() variant
It has to iterate though all the files/directories within the object, it has to do this one at a time until all the content is consumed.
2024-02-02 11:47 AM
Like this?
2024-02-02 12:20 PM
IT WORKED,
I added a line to break:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.