STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5A5: AZURE RTOS and 1ms ticks - how to set?

I am confused: I want to have 1ms AZURE RTOS tick timer - but no idea how to set.What I see:AZURE RTOS defines 10ms tick timer (UX_PERIOD_RATE, TX_TIMER_TICK_PER_SECOND)I see as well, when using tx_thread_sleep(1000); - it sleeps 10 second (not 1) - ...

tjaekel by Lead
  • 6825 Views
  • 4 replies
  • 3 kudos

Resolved! STM32L4xx Low power modes

Hi all,I am designing an application on a STM32L431. I need to consume the least amount of power. The MCU will have to use the CAN module both in transmit and receive mode. The reference manual does not give too much details on how the lower power mo...

bareil76_1-1707925217793.png
bareil76 by Associate II
  • 2185 Views
  • 1 replies
  • 1 kudos

Resolved! STM32WB55 THREAD Change Thread Config

Hi,My thread starts working with the features I mentioned below:    panID = 0x2222U; channelNB = 12U; networkKey = (otNetworkKey) { .m8 = {0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99, 0xAA, 0xBB, 0xCC, 0xDD, 0xEE, 0xFF} };    ...

osDelay returns too early

Hello There, I'm working on an app utilizing STM32H7A3 with CMSIS-OS2.I'm facing a problem with osDelay(). Most of the time it returns too early than the actual delay. While HAL_Delay() always works fine.I have debugged osDelay(3500) with oscilloscop...

KAgga.1 by Associate III
  • 8790 Views
  • 13 replies
  • 3 kudos

Resolved! How to get a ADC resolution?

I have the following code that I call from a freertos task scheduled with a period of 100 ms.It reads the voltage applied to a pin and return the voltage value as a float.   float pinin_pv(void) { /* Return the pin voltage in the interval [0, PIN_VOL...

ubaldot by Senior
  • 3560 Views
  • 6 replies
  • 5 kudos

1. If we are logging data for the long period (48hour or 96 hour) Sometimes garbage file create in sd card other than our create file. 2. Some times file corrupt and not open on the computer. What is the reason of this issue??

Dear Community Member, I am working on the data acquisition and logging is SD card. In this project i am using stm32l452RET6 uC to interface SD card in SDIO mode with fatfs. It is working file when we are logging for the shorter time. I am creating o...

KPras.2 by Associate III
  • 6951 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.