STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L152RET6 - BOR Setup failed

Hi folks, this is my first post here on this forum and I expect to find an answer to this issue I currently have.Just so you know, my current hardware setup involves an STM32L152RET6  MCU on our custom board which we have been able program using a Nu...

Resolved! LAN8742A no clock output

HiI am using STM32H753VIT6 together with LAN8742A.I have some questions regarding the setup.1. My schematic for the LAN8742A is shown in the picture below. I plan to use the PHY to generate the clock. To my knowledge this requires a pulldown resistor...

tyassin_0-1708635821688.png
tyassin by Associate III
  • 3526 Views
  • 2 replies
  • 1 kudos

Resolved! Unused UART Rx pin on STM32F

Dear All,on my STM32F board, i have the uart rx pin not connected/floating. Due to too many noise interrupts, I have configured UART in tx mode only and disabled RX interrupts. Is this fine? Or should the internal pull up be enabled for the RX pin? 

krishr by Associate III
  • 3108 Views
  • 5 replies
  • 2 kudos

Resolved! STM32F4 USB DFU trying to write to external memory?

Hello everyone,I'm having issues with programming a STM32F429IIT using USB DFU. Im able to program it without issue with a STLinkv3 and the hardware is fully working.  The issue is strictly when using ST-Prog, the firmware download will reach 54% and...

XD by Associate III
  • 3238 Views
  • 4 replies
  • 1 kudos

NetXDuo TCP Client Notify Issue

Hi all, I am currently running tcp echo client example code from st on a NUCLEO-H563ZI which I have got working send and receiving messages over TCP/IP I am trying to get nx_tcp_socket_receive_notify working however when I use the function and connec...

NApps.1 by Associate II
  • 2570 Views
  • 1 replies
  • 0 kudos

Free RTOS queue mechanism does not work as expected.

Hi, I have written below application. When manager task is scheduled for the 2nd time, the xStatus and xWorkTicketId get strange values as seen below.     When employee task is scheduled, xStatus gets "0" which indicates no variable in the queue wai...

demir_0-1709561271840.png demir_1-1709561406021.png
demir by Senior II
  • 3902 Views
  • 1 replies
  • 1 kudos

Resolved! LPUART can't display a large message

Hi everyone!I'm using a NucleoWB55 and the LPUART protocole to communicate with a SIMCOM module. I'm able to send via the LPUART the AT commands that I want and to receive it's answers. I'm now trying to print on my terminal the content of my web pag...

terminal ST.png WhatsApp Image 2024-03-05 at 10.40.52.jpeg variables commandes.png fonctions AT.png
Fannyrsy by Associate II
  • 2568 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.