STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Transmitting and receiving custom serial bitstream

Hi Community, 1) I have to demodulated a continuous bitstream of 201bit (1ms per bit) sent by a host to my stm32F401RE. Which peripheral would you suggest to use?2) If I have to transmitt and receive custom serial data  in half duplex with clock in T...

FAJOL.1 by Associate III
  • 2491 Views
  • 4 replies
  • 0 kudos

Using LwIP's sockets with CubeMX ?

I would like to use plain sockets in my non OS STM32 application.  LwIP provides plain sockets.  I have used them in ESP32 applications where they work well.LwIP sockets are not an option in CubeMX as far as I can tell.   One can manually enable sock...

Someguy by Associate III
  • 2719 Views
  • 2 replies
  • 2 kudos

stm32f401ccu6 disconect while programming (NOOB HERE)

Hello guys Im new here, sorry if I posted to wrong post.Im trying to program stm32f401ccu6 with existing .bin file. I tried via ST-LINK V2 (clone) and Im getting ''('' where serial numbers should be. When connected via USB C the board get connect to ...

ak1ca_0-1709976610279.png ak1ca_1-1709976737989.png
ak1ca by Associate
  • 1059 Views
  • 1 replies
  • 0 kudos

fast data transmission from MCU to PC

 What is the fastest way to transfer data from an MCU to a PC?I have an stm32h723zg that I want to use to transfer 40Mbits/sec data to a PC, but I am not sure what is the way to achieve this I tried USB CDC but got only 0.5Mbits/sec due to the limita...

DEska.1 by Associate II
  • 3429 Views
  • 3 replies
  • 1 kudos

STM32 Nucleo 767ZI FreeRTOS benchmark

Im currently porting a CPU performance benchmark from ESP32 to STM32 that uses FreeRTOS. Im unable to make it work due to some errors that continue appearing that might suggest there is a stack overflow, but increasing the stack size doesn´t help.Deb...

Alex2968 by Associate II
  • 3120 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.