STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about STM32H747I-DISCO audio recording example

I'm working on the STM32H747I-DISCO board. While trying out how the recording works on the board, I downloaded and built the latest version 1.11.0 from: https://www.st.com/en/embedded-software/stm32cubeh7.htmlSpecifically, the code in: .\STM32Cube_FW...

ivy by Associate
  • 3299 Views
  • 3 replies
  • 1 kudos

Resolved! EEPROM emulation problem on STM32H563

Hi,I'm facing problem in reading data from EEPROM, which was written before power cycle.EE_Init() always causes formatting of EEPROM irrespective of EE_CONDITIONAL_ERASE or EE_FORCED_ERASE parameter passed, resulting in erasing the previous dataConfi...

Resolved! I2C using the HAL library in the IT mode.

I have implemented a basic I2C between STM32H7 (Main) and STM32F4 (Secondary) processor. I am using an array of size 6 to transmit from the Main CPU to Secondary CPU using I2C in IT mode.The HAL API for I2C requires the data_buffers to be of size uin...

Sahilsb7 by Associate III
  • 5207 Views
  • 4 replies
  • 1 kudos

Resolved! Custom initialization of peripherals

Hello,I am working with timers in a stm32 project. In the generic INIT function that is generated using the .ioc file important functions like HAL_PWM_Init(),  HAL_TIMEx_MasterConfigSynchronization() etc are understandably called outside the user cod...

Avi_8 by Associate II
  • 2142 Views
  • 2 replies
  • 4 kudos

Resolved! SFR view, wrong address of registers bit field?

I am working with STM32G474RET6U MCU and I would like to check the values of bit filed EXTSEL (ADCx->CFGR.EXTSEL) the problem is that according to SFR view this bit field starts on 6th bit of CFR register, but according to the reference manual it sho...

0693W00000WJYL9QAP.png 0693W00000WJYKuQAP.png
GHrib.1 by Associate III
  • 1689 Views
  • 4 replies
  • 0 kudos

Problems with osMessageQueue

Hello.I'm using the STM32U5A9J-DK development board to work on a project to display UART data on the screen textArea, and I've made sure that there are no problems with the communication between the PC and the STM32 UART, and with the process of Mode...

jessie_chiu_0-1711089386454.png

Resolved! STM32F107+LWIP(2.0.3)+freeRTOS not work

i use STM32F107+LWIP(2.0.3)+freeRTOSI wrote the program with the help of the following document :https://www.st.com/resource/en/user_manual/um1713-developing-applications-on-stm32cube-with-lwip-tcpip-stack-stmicroelectronics.pdfAfter connecting the c...

HKabi.1 by Associate II
  • 8850 Views
  • 13 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.