STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F207ZG , USB HID as device not working

Hi,I am using Nucleo-F207ZG development board and trying to make it as keyboard type device.I have changed 0x01 in 'USBD_HID_CfgFSDesc' And also changed 'HID_MOUSE_ReportDesc' for keyboard.I have attached screen shot of .ioc fie settings, please guid...

jjmamtora_0-1718016929136.png jjmamtora_1-1718017069289.png
jjmamtora by Associate II
  • 2024 Views
  • 1 replies
  • 0 kudos

EWI Interrupt

I am trying to generate an EWI Interrupt from the WWDG on a WB55.I have  WWDG_EWI_ENABLE set, I have global interrupts enabled and I have WWDG_IRQn enabled.I can generate resets from the WWDG, but I never get an EWI interrupt. I checked in the link m...

TWood.4 by Associate III
  • 1461 Views
  • 1 replies
  • 0 kudos

stm32f407 dual ADC Simultaneous sampling issue

dual adc input gpio is pc4(ADC1 input)、pc5(ADC2 input).ADC1 gpio pc4 input sine wave,ADC2 gpio pc5 input is floating.when dma mode use ADC_DMAAccessMode_2,ADC2 last sample data is also sine wave,why?when change dma mode is ADC_DMAAccessMode_1,ADC2 re...

xu2 by Associate II
  • 2010 Views
  • 3 replies
  • 0 kudos

Resolved! USB PD sink

Hi Team, I want to work on USB PD sink , which board would be suitable?, I'm trying for 28V 5A power. I think the firmware for this specification is not available yet. Even though i want to try on. Would you suggest me any board? Is STM32L562 would b...

NITHIN by Associate III
  • 4909 Views
  • 7 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.