cancel
Showing results for 
Search instead for 
Did you mean: 

43: error: invalid use of incomplete typedef 'uart_handle_t' {aka 'struct uart_handle'}

sai_sankar_rao_R
Associate II

Hi all,

I am a new member to stm controllers.

i am using B-L072z-LRWAN1 & SUB IOT STACK.

While iam using wrapper class functions i am able to see the output of my code

uart_handle_t* uart_0;

uart_0 = uart_init(0,9600,0);

uart_enable(uart_0);

uart_send_byte(uart_0,0x07);

 

but while i am trying to send data using hal function i am facing this

error

 

error: invalid use of incomplete typedef 'uart_handle_t' {aka 'struct uart_handle'}

 

code

uart_handle_t* uart;

uart = uart_init(0,9600,0);

uart_enable(uart);

uint8_t data = 0x55;

uint8_t *pdata = &data;

HAL_UART_Transmit(&uart->handle, &data, 1, HAL_MAX_DELAY);

 

but please also have look at wraper class code

void uart_send_byte(uart_handle_t* uart, uint8_t data) {

HAL_UART_Transmit(&uart->handle, &data, 1, HAL_MAX_DELAY);

}

 

please help, thanks in advance

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
STTwo-32
ST Employee

Hello @sai_sankar_rao_R 

Can you give more details about your issue (detailed description of the project, Error context, Some creenshoots,...).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

sai_sankar_rao_R_0-1718001581929.png

 

sai_sankar_rao_R_1-1718001592163.png

 

You need to show your uart_handle_t structure. It's probably missing UART_HandleTypeDef and if handler is it, I don't see where you initialized it with a instance?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Andrew Neil
Super User

Please use this button to properly post source code:

AndrewNeil_0-1718034154289.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Do you have the actual typedef, or any, in this file or it's includes?

If not, probably wants you to explicitly describe the pointer

struct uart_handle_t* uart_0;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.