STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5A5: DMA to SAI2 does not work - why?

I want to send audio samples (received via SAI1 from PDM MIC) to SAI2_SD_B as SPDIF out. It does not work, because: the DMA does not seem to write the DR in SAI2: the memory is filled with audio samplesthe DMA seems to run (I get the HAL_SAI_TxCpltCa...

tjaekel by Lead
  • 1637 Views
  • 1 replies
  • 0 kudos

Resolved! SDMMC + FATFS on STM32H753Zx

Hi,   i go to start SDMMC1 in STM32H753z, is any sample code? can please provide.   in SDMMC i need to use FATFS APIs or SDMMC APIs ? i am confusing please help me.   when i debug the below code i am can n't access it stop at f_mount() starting only....

Naresh_ by Associate III
  • 4781 Views
  • 6 replies
  • 0 kudos

STM32 LPUART INTERRUPT IS NOT WORKING

Hi,I am developing on stm32l011 board and I am facing issue about UART interrupt. static uint8_t rxBuffer[32] = { 0 }; void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { /* Check if it is start command. */ if(NULL != strstr((char*) rxBuffer,...

processing audio in real time

In the next code I sample audio from the mic, play it to the headphones, then i process the data to get Mel-Spectrogram feature and then I feed the Mel feature into an AI model to recognize speech.when I enable the functions that calc the mel and the...

audi by Associate II
  • 2575 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.