STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CanOpenNode Send Data

Hello friends,I'm new to the H series and CanOpen. I found the CanOpen Node stack sample structure on Github. I did some experiments on this. But I cannot see the data.Data always comes as zero and dID =723, but my ID is 123. Can anyone help me on ho...

Yandas by Associate III
  • 3247 Views
  • 2 replies
  • 1 kudos

Resolved! Execute specific functions from RAM

Hi, I would like to know the procedure to execute specific functions from RAM.I have tried __ramfunc at beginning of the function but it requires all the subsequent functions also to be run from RAM. This would require lot of manual code updates. Is ...

nagarasr by Associate II
  • 8143 Views
  • 10 replies
  • 4 kudos

Resolved! LT6810 Library import in stm32H753 code

I am writing the code stm32H7ZIT6 based master to control slaves based on LTC6810 ic. Although, I am getting errors while importing the specific LTC libraries needed for making this setup work. I am trying to import specifically these libraries 1. LT...

img.png
hvs_learn by Associate III
  • 4669 Views
  • 4 replies
  • 5 kudos

STM32 problem with UART RX throught DMA

Hello,I am implementing the use of the DMA for receiving data from the UART on a board with an STM32G491 that is constantly receiving data at 19200 baud.The DMA is configured in normal mode, and the receive buffer is currently of 50 bytes.Each time t...

Smark by Associate II
  • 5251 Views
  • 9 replies
  • 5 kudos

Resolved! STM32F429ZI fixed Ethernet with LWIP

I hope this email finds you well. I am currently working with the STM32 NUCLEO F429ZI and encountering challenges with Ethernet connectivity. Specifically, I am looking for example projects demonstrating how to connect STM32 to Ethernet, both using a...

QuangIoT by Associate II
  • 1993 Views
  • 3 replies
  • 0 kudos

Resolved! What causes HAL_FLASH_OB_Unlock() to call HardFaultHandler()? It calls WRITE_REG(FLASH->OPTKEYR, FLASH_OPTKEY1); and jumps directly to HardFaultHandler().

The HAL_FLASH documentation is especially poor. There in no overview of what you have to do. You would think (because of lack of anything saying different) you have to HAL_FLASH_OB_Unlock()HAL_FLASH_Program(...)HAL_FLASH_OB_Lock()The first command H...

KiptonM by Lead
  • 19447 Views
  • 38 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.