STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bug in STM32H7 OSPI HAL Drivers RX DMA code

Hi there,just found out, that there's a severe bug in STM32Cube_FW_H7_V1.11.2, file stm32h7xx_hal_ospi.c at line 1599 (Function HAL_OSPI_Receive_DMA), which prevents the OSPI DMA Receive mode from working correctly:   /* Enable the transmit MD...

hknief by Associate
  • 1398 Views
  • 1 replies
  • 0 kudos

HAL_I2C_IsDeviceReady error at 100khz

i am getting sistematically the exact problem described in this post https://github.com/STMicroelectronics/STM32CubeG0/issues/46 at 100kHz I2C frequency. I am using a nucleo with stm32fg031. Even tho i have set up 5 trials, i only get on my analyzer ...

kuzi_996 by Associate
  • 1397 Views
  • 2 replies
  • 1 kudos

OTA implementation stm32l072

SO I HAVE STARTED MY PROJECT WITH STM32L072 SERIES WHICH IS HAVING 192B FLASH 64 PIN IC along with bluenrg-m2sa. my concern and doubt is regarding implementation of ota feature to stm32l072 ic which i never implemented and work on before and also the...

STM32F0 bootloader

Dear Members, I'm using the STM32F030CC controller for my RTOS-based project and currently developing a bootloader for it. The application code has been relocated to 0x08004000. The bootloader successfully jumps to the application, but after initiali...

Sid_sid_2-1728297669622.png
Sid_sid by Associate II
  • 5380 Views
  • 10 replies
  • 0 kudos

netxduo link state not initialized properly

Dear Community,We're just building up a product with NetXDuo on a STM32H563 having some issues with the Link-Establishment.We use newest CubeMX (6.11.0) with newest Firmware-Package (1.2.0) to generate the init-code and use the same PHY as in the Eva...

stst9180 by Associate III
  • 3755 Views
  • 4 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.