STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX - Composite USB device - CDC ACM and MSC

I'm trying to develop an application for the STM32H750 using USBX to implement two classes on the same USB device: CDC ACM and MSC. I've managed to get each one working individually, but I'm having trouble combining them. When I connect it to a PC, n...

TIM_BRK PWM shutdown

hi, im using stm32g474vet6 tim_bkin for pwm shutdown through external pin, when im normally using pwm only tim break interuppt is happening, pwm is shutting down but if im using same timer in triggermode for another timer and pwm generation, tim_brk ...

USB-PD default role initialize & change

Hi supporter,I have one question: I want to change Port Role when no cable connect, can I do it?my behavior:Init usbpd with default role is Sinkwhen my application running, I see my adapter plugin, I want change my port to sinkCan I do that?

H V N D by Associate III
  • 4284 Views
  • 6 replies
  • 0 kudos

HTTPS server over USB

I need to set up an HTTPS server over USB using the STM32U5A5 microcontroller.  I do not see an example of this configuration.  There are examples of HTTP servers for other microcontrollers using USB, but not HTTPS and not for the U5A5.  Is it possib...

FileX help

Platform Nucleo-H563ZICubeIDE V1.15.0ioc file attachedI'm starting with a simple app to get fimilar with the new Middleware.I created a new STM32 app and enabled ThreadX and FileX.I also changed the recommended settings for IChache and the system tim...

KKobe.1 by Associate
  • 3647 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.