STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA -> MDMA chaining stm32h7

Hello everyone, Context :  I am having troubles chaining the DMA1 and MDMA of the stm32h755, more precisely, I am looking for the following data flow when reading data from SPI, the SPI being regularly triggered  :  SPI -> DMA1 Channel3 -> SRAM -> MD...

STM32F469I-DISCO CS43L22 Audio Codec

Hi! I am trying to generate a sine wave on my CS43L22 audio codec chip and use the included stereo jack on my STM32F469I-DISCO board. I'm using the STM32Cube IDE. There is one .WAV player example that I can't get to build in the IDE that's closely re...

STM32G4 trigger SPI-DMA transfer with timer

Hello,I want to trigger a SPI-transfer with a timer. Its like in this post:https://community.st.com/t5/stm32-mcus-embedded-software/stm32g4-trigger-dma-request-from-spi-to-memory-with-timer/td-p/726370but I want that an output compare of a timer that...

Smallface by Associate II
  • 2058 Views
  • 3 replies
  • 0 kudos

RTC Timestamping Delay?

Hi everyone,currently I am working with an STM32L431 on a project that timestamps incoming IEEE802.15.4 frames via an AT86RF233 radio. The radio module is configured to issue an interrupt when a message is received and this interrupt signal is connec...

Resolved! RTC Wake-Up from Stop3 on STM32U545RE

I would like to use the Stop3 low-power mode on an STM32U545RE (NUCLEO-U545RE-Q board) and to wake-up the device by the RTC. I have a working example for Stop2 mode for which I largely used the inspiration from the stm32u5 workshop. But when I replac...

TNaum by Associate III
  • 18200 Views
  • 28 replies
  • 4 kudos

Resolved! Non Blocking programming

I have a STM32F411 board connected with a GPS module connected onto USART2I also have Tim1 and Tim3 configured for PWM generation on their channels respectively.I am running a list of commands (from an array) to execute line for line.Most of the exec...

techdesk by Associate III
  • 10509 Views
  • 23 replies
  • 10 kudos

BUG in AZRTOS 6.4 NetxDuo v3.3

in file app_netxduo.cfunction static VOID nx_app_thread_entry (ULONG thread_input){ ..../* wait until an IP address is ready */ if(tx_semaphore_get(&DHCPSemaphore, TX_WAIT_FOREVER) != TX_SUCCESS)blocks code executionas in function tx_semaphore_create...

mbarg.1 by Lead
  • 2400 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.