STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Running Zephyr RTOS on STM32F303CBT6

I have a custom board with an STM32F303CBT6 MCU with an external 16 MHz oscillator, but I am unfortunately not able to get Zephyr RTOS to successfully boot.From the KConfig options, it does not look like the specific variant of F303 is supported. It ...

sbend by Associate II
  • 2380 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE only running code from one project

Hello all, I am currently working with the STM32CubeIDE. I wrote a program that didn't end up working but concluded the code was fine after reviewing it. I tried copy and pasting the code into a different project within the IDE, and it works just fin...

dj-b by Associate
  • 2390 Views
  • 3 replies
  • 2 kudos

Resolved! Problem with pdm2pcm library in vs code

Hi,I am struggling to make PDM2PCM library work. My projects build without issues, but when I upload them to the board , program executes until it reaches PDM_Filter_setConfig function (tested with breakpoints). After that, it goes to infinite loop c...

baator025 by Associate III
  • 1878 Views
  • 2 replies
  • 1 kudos

Resolved! stm32f469 discovery USB HOST CDC

Moved from the Motor Control forum as this has nothing to do with motor control. i am using stm32f469 discovery with architecture um1932, in MX i configured for Host only host CDC class for full speed (FS) my clock configuration is also correct (48m...

Resolved! Help Understanding BSP_COM for Communication

Code formatting applied - please see here for future reference.Hello everyone,I'm currently working on an STM32 project using the NUCLEO-G431KB board. I've come across the BSP_COM API in the STM32Cube firmware, which seems to be an abstraction layer ...

jin96 by Associate
  • 4395 Views
  • 2 replies
  • 3 kudos

Resolved! Understand SD Card detect pin initialization

Hello,I would like to understand the code to carry out my software integration :  /* Configure SD pin detect */ __SD_DETECT_GPIO_CLK_ENABLE(); __HAL_RCC_PWR_CLK_ENABLE(); And This refers to lines of code that I am lost, for the first line ...

DYann.1 by Senior II
  • 11499 Views
  • 36 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.