2025-01-10 1:55 AM - last edited on 2025-01-10 2:41 AM by Peter BENSCH
Moved from the Motor Control forum as this has nothing to do with motor control.
i am using stm32f469 discovery with architecture um1932, in MX i configured for Host only host CDC class for full speed (FS) my clock configuration is also correct (48mhz for USB) also i codded to transmit data to USB device which is motor controller , i am getting application ready state and USB_OK state after transmitting some data over USB but the device is not responding, what will be the reason. but when i do the same by using stm32f469i example code provided by stm it is working .
i need to check the HOST is transmitting or not how can i ensure this. please someone suggest me what are the procedure i need to follow for configuring and debugging the USB HOST CDC
Solved! Go to Solution.
2025-01-10 11:22 AM
Hello @Abhishek_nr ,
Did you enable USB Host: "USB_OTG_FS" in Host mode?
Make sure to configure the USB Host CDC Class:
You can check and follow the video of USB training: STM32 USB training - 11.1 USB VCP host labs
2025-01-10 11:22 AM
Hello @Abhishek_nr ,
Did you enable USB Host: "USB_OTG_FS" in Host mode?
Make sure to configure the USB Host CDC Class:
You can check and follow the video of USB training: STM32 USB training - 11.1 USB VCP host labs
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.