STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SDIO, USB Mass Storage, and Mac

Hi! I am trying to learn about interfacing with an stm32f405 as a USB Mass Storage Device. My (homemade) development board has an onboard microSD card slot, and so I would like to present the card as my mass storage. I'm running into some problems wi...

sb_st by Senior II
  • 1541 Views
  • 1 replies
  • 0 kudos

Resolved! Circular dependency in HAL driver for STM32H5.

Hi!I have a project that will not compile due to "error: 'HAL_StatusTypeDef' does not name a type".The project uses STM32H563 and includes file stm32h5xx_hal_conf.h.The HAL_RCC_MODULE_ENABLED and HAL_GPIO_MODULE_ENABLED are defined.When looking into ...

Imre by Associate III
  • 1281 Views
  • 1 replies
  • 0 kudos

STM32 FATFS with SPI FLASH

I am trying to interface a SPI flash from Winbond (W25Q64JV) with FATFSI have no previous experience with FATFS.I initialize FATFS in CubeMX with the option "used-defined" and modified the MAXIMUM and MINIMUM Sector Size to 4096, as it is the smalles...

mbedtls vs wolfssl

Hello!I need to set up an STM32H745 to make an HTTPS request. In the last few weeks, I have configured LWIP using this example (https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308) and se...

RafaelS by Associate III
  • 3859 Views
  • 4 replies
  • 2 kudos

Resolved! Get external I2C3 working on Sensor Tile.Box Pro

I have a Sensor Tile.Box pro and I want to communicate using I2C to an external peripheral using the PG7 and PG8 pins, which are the I2C3 SCL and SDA pins. However I am unable to get as much as basic GPIO working on those two pins, let alone I2C.I ha...

Mantis by Associate
  • 1492 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.