STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Azure IOT Porting STM32H735G-DK

Hi currently i am using STM32H735G-DK board and i need to integrate with azure IOT via ethernet  1. From .Ioc file i have  enabled  MQTT,msns,dns,dhcp,sntp,cloud and i have added Nx azure related files and azure c sdk and the file structure as attach...

avinpat_8_0-1743752576150.png avinpat_8_1-1743752608049.png
avinpat_8 by Associate III
  • 943 Views
  • 0 replies
  • 0 kudos

STM32U073C8T6 USBX CDC ACM

I want to read and write data from the serial port with the help of the usbx module with STM32u0. However, when I insert the usb, it gives an unrecognised usb error. I downloaded and installed the usb virtual port drivers from the ST site, but I coul...

OŞeno.1 by Associate II
  • 1158 Views
  • 2 replies
  • 0 kudos

DMA not resuming after stopping

Hello,I am currently using the Hal library to do send and receive I2S signals over DMA. I am constantly calling the DMA receive and transmit functions, because I cannot figure out how to work it in circular mode. I am struggling because whenever I st...

L42Liam_1-1742062985097.png L42Liam_3-1742063084487.png L42Liam_1-1742063249226.png
L42Liam by Associate
  • 1161 Views
  • 1 replies
  • 0 kudos

STM32F303 SPWM Generation

Hello,I designed a BLDC motor driver for myself and I am currently in the software phase.I am using the 1st, 2nd and 3rd channels of the TIM8 timer for 3 phases, but I do not have any information about how to create SPWM in stm32 or how to trigger th...

Sergen by Associate III
  • 6015 Views
  • 7 replies
  • 3 kudos

Resolved! ETH on STM32H743 with Zephyr

Dear,I'm trying to use the ETH with Zephyr RTOS 3.5.99. It was built the samples/net/dhcpv4_client sample, however, I tried to build others examples from samples/net/socket, such as echo and echo_client, but was impossible.I would appreciate it if an...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.