2021-03-03 5:48 AM
2021-03-03 7:41 AM
Largest one I've used/test to capacity was 400GB, on multiple STM32 platforms (F4, L4, F7, H7..), and with FatFs builds that work properly..
Could probably get the F1 to work if I could find one with an SDIO interface, as the SPI is slowww..
2021-03-03 6:01 AM
This depends on the firmware (like FatFS), not the controller.
Any type with SPI will do.
2021-03-03 7:41 AM
Largest one I've used/test to capacity was 400GB, on multiple STM32 platforms (F4, L4, F7, H7..), and with FatFs builds that work properly..
Could probably get the F1 to work if I could find one with an SDIO interface, as the SPI is slowww..
2021-03-03 7:49 AM
Can i use SDIO/MMC interface and SPI interface irrespective of firmware? Or using which interface is suitable for large memory?
2025-04-07 5:17 PM
Any official tutorial from STM on how to write firmware to access SD card using SPI?
I found this one, however it uses SDIO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.