STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change driver SPI to DMA_SPI

Hi everybody,I training today to the screen qith the driver ILI9341.I use a library find the net.If i use the SPI in normal mode (pooling) everyhting it's ok.But the time to fill is very long ( like 2 second aprox.). SO i would like use the DMA to se...

JJoao.1 by Associate III
  • 1434 Views
  • 2 replies
  • 0 kudos

STM32 custom Bootloader

Dear community,My device is a logger. the configuration is over USB (UART vcp) via a web interface.i'm able to connect it, to configure it and store data correctly.i'm using a stm32L05x (whithout embeded DFU) and ,important, no external reset button....

jlecl.1 by Associate III
  • 3551 Views
  • 8 replies
  • 5 kudos

After STOP2 Mode Wake-Up

STM32L496VET6 – EXTI Not Working After STOP2 Mode Wake-Up1. Part NumberSTM32L496VET6, LQFP100Custom-designed hardware (not a development board)2. EnvironmentIDE: STM32CubeIDE v1.15.0STM32CubeMX: v6.11.0HAL Driver Package: STM32CubeL4 v1.18.0Toolchain...

Chintu by Associate II
  • 947 Views
  • 1 replies
  • 0 kudos

Free-RTOS and mDNS

Hello Community!I'm busy with a project that needs support for mDNS, after a long search i can't find any documentation howto implement mDNS on a Free-RTOS system. The examples provided by ST are not aware of any OS (I Think).Can someone share some i...

JDWBE by Associate III
  • 1982 Views
  • 4 replies
  • 1 kudos

Resolved! problems with the RTC WakeUp.

Moved from the Feedback Forum.The Feeedback Forum is not for product questions.Hi,I'm using Keil platform for programme my STM32 L073RZT6 and I am making it in bare metal. I would like to wake up the STM from any sleep mode using and interruption fro...

Flash with bootloader uart issue stm32f405

Hi,I'm trying to flash overt build in uart bootlader stm32 slave device. Here is my setup :Master STM32F4 with tinyUSBSlave STM32WLE5 device Master and slave are connected together over uart. Master has control of boot0 and reset ligne of slave devic...

SBaro.11 by Associate III
  • 3746 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.