STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Changing HSE and LSE source when CSS

Hello all,We are currently using the STM32G0B1RE in our design, where both HSE and LSE external oscillators are used. The PLL is configured to multiply the 8 MHz input to 64 MHz. All clock configurations are performed via STM32CubeIDE and HAL, and th...

Wadeva by Associate III
  • 1433 Views
  • 1 replies
  • 0 kudos

I2S Microphone Output Problems

Hello,I am a beginner trying to create my first STM32 project using the STM32F407G Discovery Board. I am trying to receive audio input through I2S, delay one of the channels, and then output the result to the audio jack. I can get a simple sine wave ...

Resolved! USBX Standalone example for CDC_ACM

Hi,I am implementing CDC ACM on STM32C0x series with USBX standalone. I searched for many examples but could not find a single example for USBX standalone for CDC ACM. There are examples with USBX standalone for HID Mouse. Wherever, I find example of...

PPate.1 by Associate III
  • 2994 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.