STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F072RB ADC DMA 8 Channels

 Hi, I need to read 8 channels through the ADC in DMA circular mode, to check the channel status readd I put all channel to GND from nucleo board and two channels (ADC_IN2 on PA2 pin and ADC_IN3 on PA3 pin ) doesn't give me the correct data, you can ...

Screenshot 2025-04-23 150941.png shared image.jpg
Melxo by Associate II
  • 3496 Views
  • 7 replies
  • 1 kudos

Resolved! X-CUBE-AUDIO-KIT Audio Latency

Hey all,I was just reading out the new release of the X-CUBE-Audio-Kit and it says:Configurable latency mode and audio buffer sizes adjustable down to fractions of millisecondsDoes anyone know the lowest latency that can be achieved?I'm looking to po...

LWIP 2 interfaces issue

Dear colleagues, hello! Question about LWIP. I have two network interfaces, one on the QCA 7000 chip via SPI, the second on LAN 8742, installed on the debug board. I use the Socket API. The problem is as follows: The server is running on one interfac...

Ivan4S4 by Associate II
  • 2958 Views
  • 9 replies
  • 2 kudos

CubeIDE arm-none-eabi-gcc Toolchain sources

Hi,I am currently working on a build container for my project and I’m using the ARM toolchain (arm-none-eabi-gcc) from ARM Developer sources:  https://developer.arm.com/downloads/-/arm-gnu-toolchain-downloads .Do you have an authless link that provid...

lotou by Associate II
  • 4227 Views
  • 1 replies
  • 2 kudos

FLASH_TYPEPROGRAM_FAST fails in G0B1

I tried to use FLASH_TYPEPROGRAM_FAST in a G0B1 but is not working after a page erase. I suppose it will work with mass erase but not tried. Only works FLASH_TYPEPROGRAM_DOUBLEWORD. I've also tried to make my own function to write only 32bits modifin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.