STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Optimizer problem with USBPD

Hi, I have an USBPD sink application created with CubeMX that can be found here:https://github.com/ThiRom/H563NucleoUSBPDSink   The project can be build using cmake. If the project is build using Debug configuration, it works. But using Release it sh...

USBPD.png
RomThi by Associate III
  • 614 Views
  • 8 replies
  • 1 kudos

GPDMA in Linked List with OCTOSPI

Hi all !I'm trying to write a driver for a LevelX system to talk to a QSPI chip over the OCTOSPI1 peripheral (STM32H563). I got the chip to respond to most commands, set it up in reading / protected mode.But, later, I've spotted an issue : I cannot s...

lheywang by Associate
  • 252 Views
  • 2 replies
  • 0 kudos

EPR request in STM32G071

HelloI have my own board with STM32G071KBT6 microcontroller. I successfully comunicate with charger by PD protocol and I receive up to 21 V (PPS). But I need above 21V. I have power bank with AVS up to 28V and USB cable with e-marker (up to 240W). Ho...

Resolved! USB PD Extended Source Capabilities

Hi,How do I serve request Get Source Capabilities Extended? I'm using STM32G0B1 with a port configured as SRC.When a SINK sends the Get Source Capabilities Extended the STM PD library responds with 'Not Supported' and my code is not aware that this e...

Mulleteer_0-1776944660689.png

Resolved! Possible bug in HAL_UART_DeInit()

Hello all,There might be a possible bug in HAL_UART_DeInit(). When calling HAL_UART_DeInit() when it is already initialized could lead to CPU starvation. Assume that an interrupt fires after calling __HAL_UART_DISABLE(huart); and before huart->Instan...

bala- by Associate II
  • 832 Views
  • 4 replies
  • 1 kudos

bootloader for lpuart

is there a template for developing a custom bootloader that uses the lpuart?Has the application firmware the ability to trigger a bootloader state so I can upload the new application firmware into stm32g051g8?What are the changes that I have to do on...

Awful timeout implementation in SDMMC

SDMMC HAL driver implementation is full of timeouts like this:uint32_t count = SDMMC_CMDTIMEOUT * (SystemCoreClock / 8U / 1000U); do { if (count-- == 0U) { return SDMMC_ERROR_TIMEOUT; } sta_reg = SDMMCx->STA; } while (SOME_FLAG_NOT_SET);I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.