2024-11-26 4:26 AM
Hi all,
I have just found a severe error in FileX that looks like buffer overrun in fx_file_read(), but the problem is much deeper.
This function leads to the function sd_read_data() which when invoked with use_scratch_buffer = 0 reads sectors to a user buffer directly. Unfortunately caller of the sd_read_data() (function fx_stm32_sd_driver()) checks buffer alignment for 4 only despite if project uses data cache or not. What happens next is very simple: sd_read_data() invalidates the cache for the entire buffer. If it is not aligned to cache line size then some bytes around it are also invalidated. If these bytes were dirty in cache they are lost. If the user buffer is allocated in the heap it hopelessly corrupts it.
clean_cache_by_addr(buffer, 1);
clean_cache_by_addr((((char*)buffer) + hsd1.SdCard.BlockSize * total_blocks), 1);
This will write cache lines surrounding the buffer to memory and make invalidating them later safe (of course if they do not change during the HAL call which is less probable). Please note that there is one another error in the macro: it does not add braces around arguments. So if you write clean_cache_by_addr(((char*)buffer) + hsd1.SdCard.BlockSize * total_blocks, 1);/* the SD DMA requires a 4-byte aligned buffers */
unaligned_buffer = (UINT)(media_ptr->fx_media_driver_buffer) & 0x3;
#if (FX_STM32_SD_CACHE_MAINTENANCE == 1)
/* caching requires a cache-line aligned buffers */
unaligned_buffer = (UINT)(media_ptr->fx_media_driver_buffer) & (__SCB_DCACHE_LINE_SIZE - 1);
#else
/* the SD DMA requires a 4-byte aligned buffers */
unaligned_buffer = (UINT)(media_ptr->fx_media_driver_buffer) & 0x3;
#endif
Despite of this fix my projects still crushes (but much further). I would be very thankful if any developer of the Azure RTOS pays attention to it ASAP and fixes at least this bug, and all other irregular cache handling if any. I have already lost several days with it as I first thought as usual that the error was in my code and not in OS.
Regards,
Dmitry
2024-11-26 4:44 AM
@DmitryR wrote:developer of the Azure RTOS
Azure RTOS is now Eclipse ThreadX:
So you'll find the developers at https://threadx.io/
2024-11-26 4:57 AM
2025-07-28 2:43 AM
Sad to see that it was not fixed in version 3.4.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.