2025-07-25 2:37 AM
Hello,
Working on STM32F767BITx and using Free RTOS
Enable USART2, here is the init code
static void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_RS485Ex_Init(&huart2, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
{
Error_Handler();
}
}So I can see even just after init or even after some times, the gstate == 0x20 always, and thats why unable to transmit any message over uart as it is not ready.
Please guide me what is missing here.
Thanks,
Nitin
Solved! Go to Solution.
2025-07-25 7:35 AM
Hello,
Its my mistake,
Firstly, 0x20 is a ready signal as expected, and second, I was not passing correct UART instance, which cause the communication break.
Thanks for your time
2025-07-25 7:27 AM
What hardware is this one? Are the pins being pulled to their proper idle state?
2025-07-25 7:35 AM
Hello,
Its my mistake,
Firstly, 0x20 is a ready signal as expected, and second, I was not passing correct UART instance, which cause the communication break.
Thanks for your time
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.