STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BootLoader functions use in Application

Posted on November 20, 2012 at 14:04My application requires a BOOT loader that loads an application into a FLASH device. I have created two different applications: A BOOT loader application.  start  0x08000000 A FLASH application.            start 0...

redkofka by Associate II
  • 1569 Views
  • 2 replies
  • 0 kudos

STM32F4-Discovery Board OTG

Posted on November 07, 2012 at 05:55I am trying to transfer data packets from a meter ( has a usb port) using the board to my PC. I am trying to transfer real time data packets using control transfer.  What would be the configurations for the mini a...

mshanna42 by Associate II
  • 4051 Views
  • 6 replies
  • 0 kudos

USB lib CDC example COM buffer overflow

Posted on November 14, 2012 at 16:15I want to use the VCP_CDC example in the STM32_USB-Host-Device_Lib_V2.1.0 to send ADC data, via the serial port to SciLab (a MATLAB like PC program) My problem is that the original example doesn't use any flow con...

STM32F4 USB

Posted on November 12, 2012 at 17:27Hello, I am working on a project which consist in retriving data from the Accelerometer, and then transmit it through a USB connection, So far, I quite understand how to retrive the data from the Accelerometer. B...

sidiq by Associate II
  • 2851 Views
  • 7 replies
  • 0 kudos

USBH_BulkReceiveData function blocks

Posted on November 16, 2012 at 12:34Hello!I try to implement a USB Host with 2 Endpoints in Bulk mode on a STM32F107.I use the lastest library : ''STM32 USB On-The-Go Host and Device Library V2.0.0''I wrote the class driver core like this:in USBH_In...

thln47 by Associate III
  • 1121 Views
  • 0 replies
  • 0 kudos

STM32F4 Generic USB Advice

Posted on December 12, 2011 at 09:09Hi all,I'm completely new to ARM and ST, having mainly used Microchips offering previously. Thinking it was time to branch out a bit and liking the look of the new ST stuff, I grabbed the new F4 Discovery board a ...

oli2 by Associate II
  • 3358 Views
  • 8 replies
  • 0 kudos

STM32F4-Discovery's Microphone

Posted on November 04, 2012 at 20:08Hi,I want to do a very simple project using FreeRTOS alongside with STM32F4-Discovery. I want to create a task to read from a microphone, another one will filter the mic's data and a final task would output the fi...

dfranch6 by Associate
  • 2014 Views
  • 2 replies
  • 0 kudos

Bug in Audio Codec Driver

Posted on October 20, 2012 at 10:24Hi !I'm talking about stm32f4_discovery_audio_codec.c v1.1.0 for CS43L22 .It is used in the record & playback audio demo and you can find it in the ''utilities'' folder.I've struggled a lot to make the circular buf...

bluexav by Associate III
  • 1942 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.