STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Update file on FAT SF on the fly

Posted on December 04, 2012 at 12:50Sorry for the trivial question but I need to add some data to a text file on the fly.Each time I need to open an existing file and add a line of text to it then close (to avoid data loss on power off)I'm new to a ...

FreeRTOS STM32F2xx port

Posted on November 28, 2012 at 16:01Hi,I'm trying to run FreeRTOS in my STM32F2xx application built with yagarto.Does anyone have a working reference project for such case?Actually I manage to build it but is tuck somewhere in scheduler. I'm not sur...

dimax by Senior
  • 1635 Views
  • 4 replies
  • 0 kudos

STM32F4discovery hight speed USB

Posted on November 30, 2012 at 05:15Hi:       I am using the USB part of  audio playback sample code of STM32F4 discovery. In waverecorder.c I customized the recorder_update() function. I think it stores data at the rate of 12Mbps in USB. M i right?...

its by Associate II
  • 1005 Views
  • 2 replies
  • 0 kudos

STM32F207 - LWip on FreeRTOS - correct priorities

Posted on December 02, 2012 at 21:22Hello to all,Recently I modified a FreeRTOS & Lwip port from IAR systems demo in order to make it work on my STM32F207 board. FreeRtos version is 6.1.0. I used the default demo priorities i.e : RTOS kernel -> co...

abrous3d by Associate II
  • 782 Views
  • 0 replies
  • 0 kudos

STM32F105 in USB Device Mode not recognized by PC

Posted on November 30, 2012 at 08:37Hi, I am trying to connect an F105 via USB on a PC. But the F105 is only recognized when I put an external 1,5K pullup resistor on the USB D+ dataline. Unfortunately, the same MCU is also used as an USB host for s...

marten2 by Associate
  • 1923 Views
  • 2 replies
  • 0 kudos

stm32f107 ethernet tcp or udp

Posted on August 21, 2012 at 10:15hi, i am using stm32f107vc.. for ethernet programming which one is good? TCP or UDP... i just use the ethernet communication for transferring sensor data..i am new to ethernet and stm32f107...i am using dp83848... i...

DMA TX buffers for MAC

Posted on November 25, 2012 at 02:41Why application needs to copy ethernet frame to the TX buffer first and then DMA will move it to the MAC fifo? Why is it bad idea to set up DMA to read the frame directly from application? Just want to know the re...

brberie by Associate II
  • 1380 Views
  • 2 replies
  • 0 kudos

STM3210C EVAL

Posted on November 12, 2012 at 15:16Hello, I use STM3210C-EVAL board. I have to copy the files from the SD card to a USB wih the format FAT. Is there someone who can help me? Thanks in advance. #stm3210c-eval #fatfs #sdcard-fatfs #f_mount-sdcard ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.