STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A GPL+LE RTOS for STM32

Posted on August 02, 2013 at 10:12If someone wants to try ERIKA Enterprise on the board, visit this link:http://erika.tuxfamily.org/wiki/index.php?title=ARM_Cortex_MXERIKA Enterprise is the first open-source automotive RTOS released with GPL+LE. ...

d2 by Associate
  • 722 Views
  • 0 replies
  • 1 kudos

startup_stm32f4xx.s VS startup_stm32f4xx.c

Posted on July 20, 2013 at 02:53Hello everybody.I am trying to implement the Audio_playback_and_record project from the STM32F4-DISCOVERY board on CoIDE. I have managed to do so but the only way it would work is by flashing the processor using MDK_K...

Help with Ethernet configuration

Posted on July 18, 2013 at 20:18 Hello guys, I need some help. Im trying to interface a stm32f407 with a lan8720 via RMII interface using an external clock source from the PHY. I was able to measure the 50MHz sine wave generated by the PH...

USB CDC VCP help to receive Data from PC

Posted on July 09, 2013 at 20:09Hello everybody (This about USB VCP) i started an application to send and receive data from PC to STM32F4 discovery i used the titorial provided by STmicro, but the problem i'm not able to sent to the STM32F4Discovery...

STM32F437I-EVAL Board config

Posted on July 17, 2013 at 10:31Hello,I'm currently working on a project with a STM32F437I-EVAL board. I have to use ethernet, USB OTG HS and the SD card. Problem is : I don't know how to &sharpdefine and config the dedicated ports and clocks. Aren'...

xtick by Associate
  • 1453 Views
  • 3 replies
  • 0 kudos

In BOOT mode stand GPIO pins

Posted on July 02, 2013 at 18:01Dear Developers,I wrote a program which is set to a low level of PE3 Pin. BOOT mode is switched to the next step when the PE3 Pin measured high levels.This can cause serious problems in future developments. Therefore,...

wwwharry by Associate II
  • 3697 Views
  • 6 replies
  • 0 kudos

midi-usb interface STM32F4-discovery

Posted on July 15, 2013 at 15:09 Hello, I am a bachelor student who is trying to use the STM32F4-Discovery as a midi console controler as a fun project :-). I have found no usefull sites for this, most people use the  midi box from st which has a...

benjamin by Associate II
  • 1324 Views
  • 2 replies
  • 0 kudos

USB HID Mouse and Keyboard Combo

Posted on July 15, 2013 at 09:21I want to make a USB device that has to collections, one for an HID mouse and one for an HID keyboard. But in the report descriptor, I will have to use report ID's and the HOST will ask for two separate reports specif...

Problem with LWIP board fw in STM32f107

Posted on July 04, 2013 at 09:53I have 2 devices with stm32f107 connected LAN. They are server mode and their fw is same except IP setting. I can connect each one by one at first time. But after I connected all when I try to connect  first I connect...

arge by Associate III
  • 1553 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.