STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RB - USB Keyboard

Posted on November 05, 2014 at 16:20Hi All I'm working on a project which needs to send few standard USB Keybord commands to a WIN7 Desktop. It is very simple project I'm using F103 and the ST USB library and everything seems to be working fine. Whe...

miki_pf by Associate
  • 1207 Views
  • 1 replies
  • 0 kudos

STM32F417IG single ended external clock bypass

Posted on October 26, 2014 at 20:01Hi, I am looking for some info regarding the external clock bypass conditions for STM32F417IG. There was not sufficient info in the datasheet. But, in the reference manual I could find some related data regarding h...

Nucleo-F103RB + USB

Posted on November 03, 2014 at 16:33HelloI have a board Nucleo-F103RB. I cut a usb cable and connect:D+ to PA11 D- to PA12 GND to GND pin in morpho headers VCC to E5V pin in morpho headersI am using the libraries. STM32_USB-FS-Device_Lib_V4.0.0. And...

lemac by Associate III
  • 6262 Views
  • 12 replies
  • 0 kudos

STEVAL_CCM006V1 - USB mass storage mode demo

Posted on November 04, 2014 at 18:53Hi! I have one qestion, where can find firmware for the STEVAL_CCM006V1 board or any sofware sample to run the board in USB Mass Storage mode? I will be verygratefulfor your help.    #usb-mass-storage

t23 by Associate
  • 938 Views
  • 1 replies
  • 0 kudos

Olimexino-STM32 SD-Card access using SPI and DMA

Posted on December 02, 2013 at 10:39Hey Folks,after several hours of trying I stil wasn't able to find out, why it doesn't work. Google and Forum search didn't help either.Problem: SdCard access doesnt work with the built in SD-Card-Mount using SPI ...

bernhard by Associate II
  • 1600 Views
  • 2 replies
  • 0 kudos

(stm32f407) USB with fixed vbus

Posted on November 03, 2014 at 14:51good morning I 'm doing a project with a custom board , I've been able to make work ethernet, sdio,gpio and serial ports.  but I  have been troubles with usb port to make run the usb host mode with usb-storage usi...

0690X00000604w4QAA.png

STM32Cube USB FREERTOS

Posted on October 28, 2014 at 03:22STM32Cube USB FREERTOSFor practice I wish to use cube to generate FS USB (device) and 4 analog inputs with FREERTOS.  For now my target is the STM32F4 Discovery board.  Perhaps adding FREERTOS to the project was a ...

picguy2 by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.