2016-01-04 2:56 PM
Dear Community,
I have some trouble getting the HID Keyboard on the F4 running. I can only find code examples for outdated libraries. Is there any current USB HID Keyboard HAL profile available? The only recent lib I can find is for Mouse/Joystick/Gamepad HID. Some current examples would be also very appreciated.What I want to achieve is to input strings and ALT-ASCII characters to the host via USB HID keypress including modifier keys.Thanks a lot for your help!Outdated Examples: #usb-hid-keyboard2016-01-06 5:02 AM
Hi paul007,
In the STM32CubeF4 package, you may find a HID example in this folder: STM32Cube_FW_F4_V1.10.0\Projects\STM324xG_EVAL\Applications\USB_Host\HID_Standalone.It is a typical application on how to use the STM32F4xx USB OTG Host peripheral to interact with an USB HID Device such as a Mouse or a Keyboard.You can also get more details on the HID class used to access the mouse or keyboard referring tohttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00105256.pdf
(STM32Cube USB host library).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-01-07 4:48 AM
Hi Mayla,
thanks for your reply. The examples you are mentioning are referring to the MCU being a host. However I'd like the MCU to be a keyboard (device). As far as I can tell, there is no Keyboard HID Profile in the Cube HAL. I'm looking for references to how or where someone implemented something like that.- PaulWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.