STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32CubeMX] lwIP + FreeRTOS Sample Project

Posted on April 23, 2014 at 16:41Hello Everyone,I wonder if anyone has been able to get lwIP work properly?My platform consists of Open407-D baseboard, STM32F4 Discovery and DP83848 Ethernet PHY. SysClk is clocked at 168 MHz.I have been struggling w...

emeydanli by Associate II
  • 14051 Views
  • 40 replies
  • 0 kudos

Migration to FW v1.5.1 for STM32L4

Posted on June 22, 2016 at 09:28Hi,I got to know that new FW package has been released recently for STM32L4 MCUs. So I am migrating our current Firmware based on FW v1.3.0 to the same.For that, I copied files from ''<FW Install Dir>\CMSIS'', ''<FW I...

dhaval by Associate II
  • 1890 Views
  • 2 replies
  • 0 kudos

STM32F4 USB Polling interval

Posted on June 22, 2016 at 06:58Hello,Using the processorSTMF401VETx I generate the project with STM Cube: STMCube Mx version4.12.0 library STM32CubeFW_F4 v.1.10.0I used the midlewarelibraries included in the framework to develop a USB HID device.A ...

Having trouble with DFU

Posted on June 17, 2016 at 18:03Hello,I am having a problem with dfu on the STM32L476 Discovery board. For testing purposes, I generated a binary file that is 24428 bytes long such that every byte in the file is the value '0xAA'. When I download the...

UART/USART to print to terminal

Posted on June 14, 2016 at 19:00Board: STM32F407VGT OS: Ubuntu 14.04 HAL Library (Not SPL) I am having difficulties getting output from the STM32F4 to communicate with my terminal via ''cat /dev/tty*'', putty, or ckermit. I am using USART2 from PA2 ...

STM32L0 USB Connect-DisConnect Event

Posted on June 13, 2016 at 11:32Hi everyone, I developed USB Hid Class on STM32L0 series.Everthing working properly but I  could not get the USB Connect and Disconnect Event.I am using CubeMx and HAL_PCD_ConnectCallback  and  HAL_PCD_DisconnectCallb...

STM32F407 custom bootloader problem

Posted on June 14, 2016 at 14:38Hello! I am working in a project that I want to use a custom bootloader for firmware update of stm32f407, I had developed for stm32f107 and all works fine, but for STM32F407 I getting some problems. Below I posted th...

giovani by Associate II
  • 5244 Views
  • 10 replies
  • 0 kudos

STM32F407 USART2 do not receive

Posted on June 08, 2016 at 15:51Hello, I have configured USART2 to communicate as RS422. Rx is connected to PA.3, Tx to PD.5. I need baudrate 921.600 Baud. There is no problem send anything one or more bytes. I can not receive anything from Rx (PA.3...

Why are HAL Lookup tables located in RAM?

Posted on June 14, 2016 at 11:10I notice that the HAL locates some lookup tables in RAM. For example, in stm32f1xx_hal_rcc.c:uint32_t HAL_RCC_GetSysClockFreq(void) { &sharpif   defined(RCC_CFGR2_PREDIV1SRC)   const uint8_t aPLLMULFactorTable[14] = {...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.