STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Device DMA memory corruption

Posted on February 21, 2017 at 12:11Hi,I am using an STM32F7556NG microcontroller, connecting it to a host PC via USB, with the STM32 acting as a virtual COM port.I have enabled DMA, an I have noticed very strange behaviour. By supplying a address 0...

FreeRTOS STM32 tick

Posted on February 20, 2017 at 12:26Hi, I'm trying to use FreeRTOS with a STM32F401RE Nucleo64 board. I have all the project files in place and the project compiles fine. But I'm trying to use the HAL_Delay() routine from the Cube HAL but I'm runnin...

USART - reading 1 byte at a time

Posted on February 19, 2017 at 13:39Hi,I need to parse incoming data from UART, with unknown length.The packet length is sent within the packet, so I need to parse the packet as it arrives.So - I need to read 1 byte at a time, and parse the packet w...

Custom Bootloader STM32L151x

Posted on February 17, 2017 at 17:17Hi community,I would like to know if it's possible to create my own bootloader for STM32L151x.Where I could find info about it? Some code? Built-in code..?Thanks in advance.Regards#bootloader #stm32l151 #custom

Stm32F407VG USB Problem

Posted on February 18, 2017 at 09:17Hi,I am using STM32F407VG chip in my own PCB. I design MCU part of the PCB according to DISCOVERY board since it has the same controller. The board seems to work just fine. I tried ADC, DAC, SPI, USART, and simple...

0690X00000606KRQAY.png 0690X00000606C3QAI.png 0690X00000606KaQAI.png

I2C not working with usb

Posted on February 19, 2017 at 19:59Hello EveryoneI have a odd problem. I am using USB device to store data and reading data on same MCU(Slave) from other MCU(Master) on i2c but after after 2 or 3 transfer of data i2c stops working on slave mcu.What...

How to Debug FreeRTOS?

Posted on February 16, 2017 at 21:38I remodeled DemonstrationProgram of ST32Cube into STM32F746G-Discovery and was able to play the MP3 in audioplayer.My MP3Program may sometimes do Stall in Error.Will there be the good method to perform of Debug in...

STM32 DFU mode loads wrong driver (Total Phase)

Posted on February 14, 2017 at 02:48Hello,When I put my STM32F4 device into DFU mode, it is recognized as a ''Total Phase PD Analyzer Update Mode'' device instead of a ''STM Device in DFU Mode''. I can force using the STM DFU drivers, but by default...

0690X00000606GAQAY.png
JacobV by Associate II
  • 3619 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.