STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l053 USB VCP not getting detected

Posted on July 29, 2017 at 11:14Hi,                 I'm currently working on stm32l053 VCP. I've done a code to initialize & start VCP driver in stm32l053 and tested it using stm32l053-DISCO board, where it works fine. I can able to detect the com p...

0690X00000607jmQAA.png
LRPS_92 by Associate II
  • 1419 Views
  • 2 replies
  • 0 kudos

HAL_UART_Transmit_IT pauses during transmission

Posted on July 28, 2017 at 22:16Hi everyone,This is not a very serious issue for my application, however, I would like to understand this behavior.In my application, when the STM receives a packet, it sends out a packet with a confirmation. The cont...

0690X00000607jgQAA.png 0690X00000607gYQAQ.png 0690X00000607jMQAQ.png
Lucas C by Associate II
  • 1921 Views
  • 3 replies
  • 0 kudos

Resolved! Development boards to use for FreeRTOS and ThreadX

Posted on July 28, 2017 at 21:48We are currently trying to port an application from Linux to ThreadX and FreeRTOS and wanted feedback from the community on which development boards would you recommend to use. Looking for a board with Cortex-M proces...

CubeL4 missing CMSIS

Posted on July 14, 2017 at 10:21Hi!I've migrated one of my projects to CubeL4 v1.8.1 and regenerated my configuration using CubeMX. After that, my project did not compile and I noticed that the cmsis drivers were missing. After a bit of investigatio...

USB Huawei modem with stm32f407

Posted on July 26, 2017 at 10:04Hi,I'm working on application that uses a USB HUAWEI MU709 modem with STM32F407. First off all, i used the usb stack from keil to  implement the CDC mode: https://www.keil.com/pack/doc/mw/USB/html/host_cust_tutorial.h...

hilwan by Associate II
  • 1615 Views
  • 2 replies
  • 0 kudos

USB CDC and MSC Middlewares integration

Posted on July 27, 2017 at 13:13Hi all, I'm using STM32L486 microcontoler and USB device. Using MSC_Standalone and CDC_Standalone project example from the STM32Cube I was able to configure the USB device on CDC and MSC. Now, I want to integrate both...

IWDG and System Memory Bootloader

Posted on July 27, 2017 at 05:10Hi, everyone, I have a strange phenomena concerning IWDG in system memory bootloader.(I'm using STM32F030F4P6)In my project, I can jump to system memory bootloader using software in application,it works fine with ST's...

Zt Liu by Senior III
  • 1226 Views
  • 0 replies
  • 1 kudos

what causes ERROR_END_OF_STREAM ?

Posted on July 19, 2017 at 03:35I have a F767 and LAN8710A using Cyclone TCPmy packets are using the HTTP Get and Post methodsI send 1 packet ok,after that some packets work but others report ERROR_END_OF_STREAM??#ethernet-stm32f7

T J by Lead
  • 1289 Views
  • 2 replies
  • 0 kudos

[F2 1.6.0] USB CDC works only with -os flags?

Posted on July 24, 2017 at 03:33 Hi everyone. I have stumbled across an odd problem and would like to share it here and ask if someone knows a solution. Following scenario: I created an empty Project for my custom pcb F2 (see project's ....

usb printer class

Posted on July 23, 2017 at 13:10Hello!I want to create somthing like usb to lpt (or serial) converter to print with different old printersSo via Cube i create Custom HID project, redefine descriptors like in http://www.usb.org/developers/docs/devcla...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.