2017-07-14 1:21 AM
Hi!
I've migrated one of my projects to CubeL4 v1.8.1 and regenerated my configuration using CubeMX. After that, my project did not compile and I noticed that the cmsis drivers were missing. After a bit of investigation, I found that the firmware package zip file is about 200MB smaller than 1.7 and 1.8 and the uncompressed size is about half, only the ST-specific things are included. That means, there are no third party packages in the L4 patch, no utilities, not even BSP files. This means, that the L4 package is unusable, I had to revert to 1.8.0.
#bug #cubel42017-07-14 1:33 AM
Note to others who have the same issue: delete and redownload the patch, it solved the issue for me. For whatever reason, the patching process forgot to copy old unchanged files into the 1.8.1 firmware folder...
2017-07-28 8:57 AM
Dear
Buga.D_niel
,The issue is already reported internally and will be fixed as soon as possible.
Thanks a lot for your contribution to the enhancement of our resources and for sharing the solution with other 'STM32 MCUs forum' users.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.