STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clarity on RAM STL Tests

  I am using STM32L476JE. I wish to use STL api to test 128kb of RAM as startup test for my device. I have come across some example codes but there seems to be confusion around the subsets.If possible can you share an example code snippet for the sam...

MIPI-DSI LTDC configuration lcd

Hello everyone, I need help with a DSI + LTDC configuration.I'm working on a custom board with an STM32H747BIT and trying to drive a 720x1280 RGB888 display without GRAM, using the ILI9881C controller via DSIHOST + LTDC.Here’s the situation:I’m curre...

Optimization breaks SPI code on L562

L562 processor.  SPI1.  Blocking mode.  Two sequential writes, second write variably returns error.code:// uses CS if USE_CS is set to CS_ACTIVE (default) // CS is not used if USE_CS is set to CS_INACTIVE uint32_t HAL_SPI::Send( uint8_t* cmdpt...

Resolved! Hard Fault during tx_sempahore_get()

I have a custom board with a STMU5F7VJT, programmed over SWD, with an on board MMC and a usb connector. I am trying to access the onboard MMC with FileX and ThreadX. Using USBX, I can access the MMC just fine, and even format it from my computer, so ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.