2025-09-29 7:37 AM
I am trying to load LwIP_TCP_Echo_Server (an example project created by STMicroelectronics) onto a Nucleo_H7S3L8 Evaluation Board (produced by STMicroelectronics) and it's crashing. I had some trouble getting the BootLoader to run through to the JumptoApp function (covered under a different post) and used a workaround fix it.
I set a break point just before the jump and examined the App memory at 0x70000000 (memory mapped). It was all 0xFFFFFFFF. No wonder the code crashed. I used the STM Programmer, and the memory looked ok. Code at 0x70000000 looked like a vector table and definitely not 0xFFFFFFFF. I added the Template_XIP_Boot project to my build as described in the README.md.
I really need to get this piece of ... code to work. Like now. This stuff is basic startup operation. This is an ST example project on ST Nucleo hardware. What's going on? I've seen no other forum posts on my recent issues. Why is everyone else having fabulous success? Am I alone? What's wrong with me?
There are concepts like OctoSPI, XIP, and memory-mapped External Flash which are pretty complex, and I do not want to have to debug them (especially through the HAL).
Solved! Go to Solution.
2025-10-01 9:31 AM
Hello @JimEno,
The example works correctly. To better assist you, could you please specify the version of STM32CubeH7RS you are using as well as the revision of the Nucleo_H7S3L8 board you have?
Thank you for your collaboration.
Dor_RH
2025-10-01 9:31 AM
Hello @JimEno,
The example works correctly. To better assist you, could you please specify the version of STM32CubeH7RS you are using as well as the revision of the Nucleo_H7S3L8 board you have?
Thank you for your collaboration.
Dor_RH
2025-10-05 11:55 AM
Dor_RH,
I omitted the following step from the README.md file thinking it was only needed if I programmed my Nucleo board using the Programmer.
- User Option Bytes requirement (with STM32CubeProgrammer tool)
- XSPI2_HSLV=1 I/O XSPIM_P2 High speed option enabled
Turns out I need it. It seemed to fix not only this issue, but my previous issue
with some function timing out in the BootLoader. It was a weird symptom.
So I will consider this issue resolved. Thanks for your response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.