STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB OTG: function of CHDIS/CHENA

Posted on December 09, 2017 at 00:32I'm working with the OTG FS core on the STM32F205ZE, and having some trouble understanding the sequences used in the example code. In the manual (RM0033) under register description for HCCHAR, the CHDIS/CHENA bits...

HAL_GPIO_Init problem

Posted on January 03, 2018 at 16:05I've been some months working on a Firmware for STM32L476VG. I've made a second version of my PCB adding more hardware as 6 MOSFET controlled from MCU.The problem is with the MOSFET controlled from PE10, as seen in...

Resolved! USART VCP connections on NUCLEO-L432KC

Posted on January 02, 2018 at 16:32Hello,I just bought a NUCLEO-L432KC board. I understand that of its 2 USARTs the USART2 is connected to the ST-Link Virtual Com Port via pins PA2 and PA15.The RX pin PA15 apparently is not broken out on the Nucleo ...

FreeRTOS STM32F4 Question / Problem

Posted on December 23, 2017 at 21:40I am a beginner in both STM32 and FreeRTOS. I tried writing a FreeRTOS program logging ADC reading through serial port. I have a DMA set-up to save ADC readings in an circular buffer array, and I also have a DMA s...

0690X00000609HjQAI.png
Hz Lin by Associate II
  • 2446 Views
  • 4 replies
  • 0 kudos

USB CDC Bug in CubeMX firmware

Posted on April 11, 2014 at 10:07Hey everybody, in order to initialize a working Virtual Com Port with CubeMX on the STM32F4 Discovery, I had to change   pdev->pClassData = USBD_malloc(sizeof (USBD_CDC_HandleTypeDef)); to   pdev->pClassData = (void ...

STM32F302R6 and CAN

Posted on October 04, 2016 at 15:01 Hello. After the initialization CAN interface and call HAL_CAN_Receive_IT function (& hcan, CAN_FIFO0) there is no interruption USB_LP_CAN_RX0_IRQ Handler (); when receiving the CAN package. And accordingly mi...

ssurneed by Associate II
  • 2254 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.