STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About STM32F072 device , Problems when use HAL_SPI_Receive function of HALL in single wire and half-duplex mode.

Hlello. I want to use single wire and half-duplex mode for spi master.Init works, and HAL_SPI_Transmit function works .But it will go to timeout when call ​HAL_SPI_Receive function from HALL. it still can't get RXNE FLAG . I measured it , it didn't g...

hzhu.17 by Associate
  • 572 Views
  • 0 replies
  • 0 kudos

Resolved! Problems with custom bootloader on STM32F4

Posted on June 01, 2017 at 17:34Hello, I have some problems to implement a bootloader in a STM32F4. I searched on internet and I found coherent informations and examples, but I 'm not able to make simple test work.Here my simple code:bootloader (wri...

I2C send 0x00 and 0xFF for sensor reset

Hi,in order to reset my I2C sensor TLE493D-W2B6 A0 I need to send 4 bytes which consist of 0xFF->0xFF->0x00->0x00 . So no address or anything else, only the 4 bytes transmitted with 4 consecutive I2C accesses.Now I am using a slightly modified versio...

mx by Associate
  • 1611 Views
  • 2 replies
  • 0 kudos

How to set required voltage on STUSB4500 IC

Hello     Requirement is:we are using 3 cell(3.7*3 = 11.1V) battery in our design.so we are using charging IC for that.charging IC need 15v(max 2A) to charge LIPO battery.so we are going to use universal type c charger that Supports 5V,9V,12V, 15V an...

Apate.61 by Associate
  • 1648 Views
  • 1 replies
  • 0 kudos

To improve the copying speed from SD to USB?

Hi,Processor : STM32f429Frequency :180 MhzFatFs : ChanIn my project, I am copying the files from the SD card to the USB stick.I having the problem with copying speed. Currently a 45 MB file copies in 1.55 minutes.How to improve Speed? What are the pa...

How to use the LwIP library?

Hello,I created UDP server with LwIP stack on STM32F407.I tried example udp_echo _server. It works.Now I need send from server my own answer data in callback function.The program hangs in callback function.void udp_echoserver_receive_callback(void *a...

Peko by Associate III
  • 775 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.