STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Oscillator for USB in the STM32F413

Hello everybody!I am going to work with USB on the STM32F413 . The datasheet says:"The USB OTG full-speed controller requires a dedicated 48 MHz clock, which is generated by a PLL connected to the HSE oscillator"I would like to ensure if it can work ...

Yevpator by Associate III
  • 2054 Views
  • 4 replies
  • 0 kudos

I am trying to transmit and receive data on a STM32F7 (USB HOST CDC). After I receive and transmit bytes a few times my IN pipe shows a URB_Status of USBH_URB_NOTREADY and never reaches a USBH_URB_DONE state.

I am trying to transmit and receive data on a STM32F7 (USB HOST CDC). After I receive and transmit bytes a few times my IN pipe shows a URB_Status of USBH_URB_NOTREADY and never reaches a USBH_URB_DONE state.Any ideas as to why this might be happenin...

RPatn by Associate
  • 684 Views
  • 0 replies
  • 0 kudos

Stm23f103VET6 and Usb host FE1.1S

Greetings,Is it possible to interface stm32f103vet6 and usb host ic fe1.1s ? Actually am using stm32f103vet6 and need to attach a keyboard and usb pen drive at a same time. ​Any ideas or suggestions will be of great help .. Thanks.​

Flash Loader Demostrator for STM32F107VCT6

Hi:I' m trying to download the "Tiny_kernel_boot_loader.hex" via "Flash Loader Demostrator" on STM32's USART1.At the very first step, connection settings, it says connection fail all the time,baud rate = 115200 => not recognized device or .... etc....

CubeMX HAL - Is Thread Safe?

The CubeMX HAL library is considered and claimed to be "thread safe". One can select FreeRTOS on the CubeMX and generate a code.I am questioning whether the HAL is indeed 100% safe for using with RTOS. The HAL allows read/write to specific bits in th...

Yevpator by Associate III
  • 2425 Views
  • 3 replies
  • 0 kudos

STM32F042 Bootloader activation on Nucleo

Hy,as described and discussed earlier (https://community.st.com/s/question/0D50X00009sWdDqSAK/stm32f042-bootloader-activation) I want to use bootloader mode of STM32F042 to update STM32 firmware in a multi CPU system. I still see this way as very ele...

0690X000006CmVFQA0.png
harald by Associate III
  • 771 Views
  • 0 replies
  • 0 kudos

If there are 2x internal DACs in the STM32F407XX MCUs, why does the STM32F407VG Discovery Board need an external DAC for audio applications?

I'm very new to the STM32, so sorry if this sounds stupid. As far as I could understand looking at the datasheets, the STM32F407XX has 2 DACs, but when embedded in the discovery board an external DAC (CS43L22) is used. Why is that?

YChu.7 by Associate
  • 1308 Views
  • 2 replies
  • 0 kudos

How to generate a delay function with a 1 micro second resolution, without affecting the existing HAL_Delay 1 millisecond resolution function.

I'm using a STM32F429ZI Nucleo-144, and need a counter/delay function with 1 microsecond resolution, but want to keep the HAL_Delay function at 1 millisecond resolution for other uses.I'm looking at potentially reconfiguring the SysTick interrupt to ...

JBass by Associate
  • 784 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.