STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TCP to Modbus RTU client

Hello allI am new in this forumAnd would like to get yours help regurding adding to my working code the TCP to Modubs RTU client protocol.the code is working on STM32F103 and I intend to add to my PCB Ethernet TCP to Serial RS232 Module in order to e...

IIsha by Associate
  • 1506 Views
  • 2 replies
  • 0 kudos

Bootloader HardFault Error Peripheral

Hi guys,I'm using a bootloader. I am using 2 UART channels in the bootloader program. At the same time, I use these uart channels in the program I will install. But they don't work. The program enters the HardFault Error interrupt. When sending data ...

Hi world! by Associate III
  • 5243 Views
  • 17 replies
  • 0 kudos

Stm32 FreeRtos Internal Flash Linker Script

I have some functions to read-and write to memory to STM32F103 internal memory. This functions work on the gcc and standard linker script. When I want to use the internal flash with stm32 and freertos. FreeRtos does not allow to me access when I want...

ebast by Associate II
  • 2019 Views
  • 4 replies
  • 0 kudos

Defect in STM32Cube FW F7 V1.1.12.0 LwIP_HTTP_Server_Netconn_RTOS main.c MPU_Config() appears to be missing an invocation of HAL_MPU_ConfigRegion(&MPU_InitStruct);

After the first block of code setting up the fields of the struct argument to HAL_MPU_ConfigRegion(&MPU_InitStruct); it appears that there is a missing invocation of the above mentioned function (by comparison both with following code, and the equiva...

Sean1 by Associate II
  • 753 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.