STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Correct method of using CDC (Virtual Com Port)

Hi there,I love using Cube and being able to get a project up and running super quickly, especially because I work in an agile development environment.I am using CDC/USB/VCP for the first time on an STM32 system (STM32F070RB specifically, FYI) and wa...

0690X000006DoKzQAK.jpg
SWill.10 by Associate II
  • 892 Views
  • 0 replies
  • 0 kudos

STM32_USB_OTG_Driver v2.2.0 Availability

Hello, I am working on STM32F412 controller. We are using a previous version of the OTG driver v2.2.0 on which our most of the development works are done. We are on course of reviewing the changes on our application layer that we have developed, but ...

Possible SPI DMA bug in STM32K743IIK

I've run across what looks like a bug in the STM32H743IIK (144pin BGA) related to SPI DMA. It is a very strange one, and you can see the history of this issue on the ChibiOS forums here:http://www.chibios.com/forum/viewtopic.php?f=16&t=4140&start=80I...

tridge by Associate II
  • 2943 Views
  • 6 replies
  • 0 kudos

Resolved! I can only write to SD card once (SPI-fatfs)

I am using a stm32f407 and i use this code inside a loop:/* Mount SD Card */ if(f_mount(&fs, "", 0) != FR_OK) _Error_Handler(__FILE__, __LINE__); /* Open file to write */ if(f_open(&fil, "first.txt", FA_OPEN_ALWAYS | FA_READ | FA_WRITE) ...

NBlac by Associate III
  • 1983 Views
  • 2 replies
  • 0 kudos

External Flash of STM32L4 Through Boot Option

Hello:I wish to understand how to set up the hardware on an STM32L476Rxx device so I can flash the controller through a serial port. Is there documentation to support this, such as an app note? (unable to find anything) Any help is appreciated. Than...

Port STSW-STM32059 to other PHY

Hello community,i got the STSW-STM32059 running on a STM3210C eval with truestudio. Now i want to port it to my own PCB, where i use a STM32107RC and the 88E6161 Switch as a PHY. The PHY uses port 5, in 100 full duplex MII mode.Until now i got the c...

aMees by Associate
  • 682 Views
  • 0 replies
  • 0 kudos

Stm32f103vet6 usb bulk multi enpoint.

Hello everybody !I am working with usb bulk use libusbwin32 and hardware stm32f103vet6. I use multi endpoint EP1_IN, EP1_OUT, EP2_IN, EP2_OUT, EP3_IN, EP3_OUT, EP4_IN, EP4_OUT. But EP4_IN and EP4_OUT do not work, other endpoint working ok. Please he...

tduon.14 by Associate
  • 1608 Views
  • 2 replies
  • 0 kudos

Debugging when DMA is active...

When debugging, and when stopped at a breakpoint, does DMA or any interrupt driven process continue? If no, then debugging an incoming serial data stream (for example), can only be done after the stream is completed, otherwise you will miss character...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.