STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EEPROM EMULATION STM32f103

How can I store characters in flash memory of STM32F103 using HAL C coding?? I am able to store hex values in flash but no idea on how to save char values.

sne_123 by Associate III
  • 1022 Views
  • 1 replies
  • 0 kudos

STM32F4 USB CDC and MSC class to be used for both Device-to-Host communication and Device microSD reading ? Or only CDC ?

This question is related to the code design in such a scenario when host and device communicate over USB for two purposes: two-way communication (CDC) and also host is reading the content of the Device' microSD card. The CDC mode is required in this ...

eBirdman by Senior II
  • 1795 Views
  • 2 replies
  • 0 kudos

NUCLEO F429ZI Ethernet config on CubeMX

Posted on April 25, 2017 at 10:16Hi All,I am fighting with F429nucleo and ethernet interface. The example of firmware works well (lwip webserver).There is a pin PG2 RMII_RXERR which I cannot configure with CubeMX.On CubeMX PG2 cannot set to ethernet...

zamek42 by Associate II
  • 5140 Views
  • 13 replies
  • 0 kudos

Can USART3 on the STM32F730Z8T6 be used for the ST embedded bootloader? Are there any other specific hardware requirements other than toggling the boot pin to '1' to enter boot ROM .

I've looked at AN2606, it referencess STM32F73xxx but does not specifically list the STM32F730xx under the supported STM32F73xxx parts for the document. I am assuming this is an oversight but I wanted to be sure that USART3 would work and things will...

ARueh by Associate
  • 1130 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.