STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

identifier "xxxx" undefined

i have project code when i compile it shows identifier is undefinedBut i have included the path keil linker options and included header file also, i don't know why it shows like this.when i click the definition of VL53L0A1_GPIO1_R_INTx it doesn't go...

NS.16 by Associate II
  • 4673 Views
  • 7 replies
  • 0 kudos

Resolved! Isn't external NOR Flash memory mapped in write too ?

Hello,I tried to access external nor flash in stm32h743 eval board.After configuring it I can view the memory in debugger (IAR).But it fails when trying to access it from debugger memory view (0x60000000) - after erasing the sector.I see that the HAL...

ranran by Senior II
  • 1961 Views
  • 5 replies
  • 0 kudos

Is HAL Library/API thread-safe

I am developing software for a system (using HAL API) that communicates over CAN and I recently got into some issues related to thread-safety. I am using STM32L496ZGT6 mcu.Some background info:My main "thread" runs cyclically in a predetermined tick ...

Clock tree frequency values duplication in code

Hello,It seems that most examples (stm32cubeh7) are independent in clock tree values, which is exactly the correct way to do it, yet some of the examples are using hardcoded values duplicated from clock tree (duplication) which seems like a bad idea ...

ranran by Senior II
  • 842 Views
  • 0 replies
  • 0 kudos

identifier"I2C handler TypeDef" is undefined.

I am merging two projects .One project is wrote in stm32f401RE and another one is stm32f429i-discovery board.I have already included all path and build the project.It shows error like identifier is undefined.only one file path is not included.But i g...

NS.16 by Associate II
  • 1751 Views
  • 1 replies
  • 0 kudos

Resolved! CRITICAL: stm32h7xx_hal_tim_ex.h wrong defines

Dear STM, please fix the defines in stm32h7xx_hal_tim_ex.h as at least TIM_TIMx_ETR are either empty or wrong, according to the datasheet. Here is a short example, _NOT_ stating all incorrect positions:NOW, IN THE FILE stm32h7xx_hal_tim_ex.h in STM32...

Max Rest by Associate II
  • 1495 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.