2019-07-28 10:16 AM
Hey all,
I have a 32F469IDISCOVERY BOARD that I'm trying to use with CubeIDE, and all I'm trying to do right now is blink an LED with the HAL.
Starting from a new project, all periherals are initialized with their default settings.
In the User Code 3 loop, all I'm going is adding this code:
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_4);
HAL_Delay(1000);Which should, apparently, blink an LED. Unfortunately, nothing is happening. If I set the default mode to High or Low in the Cube configuration, I can get it to stay on or stay off--but can't manipluate it all all with code.
Again, this is with a 100% fresh project and all the manufacture peripheral settings.
Any help is appreciated. I must be missing something simple. Thanks!
2019-07-28 10:46 AM
Use the debugger, figure out if it is stuck, determine what is happening.
Make sure the SysTick is firing if that's what advances the HAL_Tick
Not really a fan of CubeMX or CubeIDE, so can't provide much direction there.
2019-07-28 11:27 AM
Thanks. How can I check if Systick is firing?
What is your recommended toolchain alternative to CubeIDE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.