STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C interrupt not triggered

I'm running out of ideas, there is no interrupt triggered when sending data over I2C.Processor: STM32L451Middleware: FreeRTOSI2C interrupts are enabled in STMCubeMx, also pins are configured for I2C.Sending data with HAL_I2C_Master_Transmit_IT():CR1:...

stm32 tcp_echoclient example

Can you please explain the following steps in detail in the the tcp_echoclient example.       /* pass newly allocated es structure as argument to tpcb */       tcp_arg(tpcb, es);       /* initialize LwIP tcp_recv callback function */        tcp_recv...

KINGame by Associate III
  • 750 Views
  • 0 replies
  • 0 kudos

USB DFU Bootloader for STM32F730

Hello,I noticed that in AN3156 (USB DFU protocol used in the STM32 bootloader), STM32F730xx MCUs are not listed in the table of applicable products on the first page. Does the F730 really not come with a USB DFU bootloader? Or is this omission uninte...

sd card cannot be accessed with SDMMC in 4-bit mode

I have set the parameter "mode" in CubeMx to SD 4 bits wide bus.But after doing so, I cannot access newer SD cards (HX) any more. Older cards (512 MB) work fine, which I assume is due to the fact that these cards do not support the 4-bit access from ...

BHoff by Associate II
  • 879 Views
  • 0 replies
  • 0 kudos

Resolved! how to use debug trace (_TRACE) ?

I found CMACRO "_TRACE" in USBPD project in STM32CubeExpansion_USBPD_F0_V2.1.0.I think I can enable usbpd debug trace feature using _TRACE. However, I can not find way check debug trace in my environment. I am using KEIL MDK ARM. Please advise.​​

I am using the HAL receive_IT and transmit_IT successfully but occasionally as the transmit is being setup part way through the receive message the receive interrupt fails to get enabled and an overrun error occurs. Does anyone have a solution for this?

I receive the data byte by byte and I can see that the only time that it fails is at the beginning of the transmit. It looks like the HAL is busy starting the transmit so it cannot re-enable the receive interrupt after the previous byte has been rec...

LAdam by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

The interrupt happend in APP but enter bootloader ISR

MCU:STM32F030C8Bootloader section:Flash: 0x08000000 - 0x08003FFF; RAM:0x20000000 - 0x200004FFAPP section: Flash:0x08004000 - 0x0800FFFF; RAM:0x20000500 - 0x20001FFFReview the map file, the interrupt vector has remapped to APP flash, but when work in ...

Dylan1 by Associate II
  • 1869 Views
  • 4 replies
  • 0 kudos

boot sequence for STM32F303E.

hi STM,i want to flash STM32F303E controller via uart. what is the procedure to achieve this?my mcu board is connected to pc via RS485. as per user manual i have to send 0x7F for uart flash. but i can't send 0x7F.so please suggest the possible ways ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.