2019-11-17 10:09 PM
MCU:STM32F030C8
Bootloader section:Flash: 0x08000000 - 0x08003FFF; RAM:0x20000000 - 0x200004FF
APP section: Flash:0x08004000 - 0x0800FFFF; RAM:0x20000500 - 0x20001FFF
Review the map file, the interrupt vector has remapped to APP flash, but when work in APP, the interrupt isr jump to bootloader isr
2019-11-17 11:21 PM
You can't remap the vector table in 'F0 as it's a Cortex-M0 core which does not have this remap - see the footnote in http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHHDGBC.html .
JW
PS. Please change your username to a normal nick.
2019-11-18 1:06 AM
As there is no SCB->VTOR register, in order to use a different vector table, you have to copy the new vector table to 0x20000000, then remap the internal SRAM to address 0, i.e. set SYSCFG->CFGR1|=0x03
See also chapter 2.5 Boot configuration in the reference manual.
2019-11-18 1:44 AM
understand, thanks.
I have changed my username
2019-11-18 1:45 AM
thanks,I try to remap as your method
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.