2019-12-11 4:54 PM
i have an STM32F303CB/CC, self-powered, doing USB. appnotes AN2606 and AN4879 apply. "A DP pull-up should be connected only when VBUS is plugged, a GPIO from the MCU is used to drive it after the VBUS detection."
nowhere is mentioned that the DFU ROM bootloader needs a specific GPIO to serve this purpose. it needs to engage the pull-up though. also I don't see a specific GPIO used for VBUS sensing...
what do I need for the DFU ROM bootloader to work?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.