STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Receive - pulse in MOSI line

The above image represents logic analyzer output when HAL_SPI_Receive_DMA is executed. My doubt is regarding the single high pulse at MOSI line. During HAL_SPI_Transmit_DMA , no issues. Is this normal behaviour? STM as Full duplex master, i have disc...

sreyas40_0-1763725623576.png

STM32N6 VENC_JPEG_Encoding issues

Hi everyone, I am trying to run VENC_JPEG_Encoding project using STM32CubeIDE on STM32N6570-DK board, but it is not saving .bmp as stated in README file. Upon further debugging I can see in main.c in function save_file() that it is only supported on ...

Understanding/Debugging Timers on STM32F4

I am having trouble understanding the behavior of the Timers on the STM32F429I-DISC board. I have an application using TouchGFX with FreeRTOS, which is kind of working as expected but the timer-based activity seems to be too slow, so I am trying to d...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.