2020-05-07 4:44 AM
Composite USB class device is not detected. It always shows device descriptor failed error.
Composite USB class (MSC+ CustomHID)
2020-05-07 5:37 AM
I don't think you need a custom driver for the composite class, just the individual ones, unless they also use built-in drivers. Not 100% sure on that.
I'd use Wireshark/USBPcap to figure out what's happening on the bus. Device descriptor failed sounds like the device isn't even sending a response to the request, not that a driver doesn't exist.
2020-05-07 10:03 AM
>>Device descriptor failed sounds like the device isn't even sending a response to the request..
I'd probably focus on validating the integrity of the descriptor, if it's not constructed properly it is going to get ignored/rejected. Check that it is being requested/sent from the device side.
2020-05-07 9:40 PM
Thank you TDK.
Yes, as you say like device is unable to send response to the host request..the enumeration itself failed.
Actually I am new to this and i am not able to understand for composite class specific to MSC+CustomHID, what are the device descriptors??
Right now I am working on STM32L4R5ZI board and I passed MSC class device descriptor.
VID: 1155
PID: 22314
Could you please suggest me what device descriptor should I used?? Or for composite class how we can get VID and PID which combine both the classes??
Thank you.
2020-05-07 9:52 PM
Thank you clive1.
Could please tell me that how I can check whether the response is sent by device or not??
It would be a great help,as I am totally new to this and not understanding it how should I proceed to debug this problem??
#define USB_MSC_CUSTOMHID_INTERFACE_NBR 2
#define USB_CUSTMHID_INTERFACE 0
#define USB_MSC_INTERFACE 1
#define MSC_EPIN_NUM 0x02
#define MSC_EPIN_ADDR 0x82
#define MSC_EPOUT_NUM 0x02
#define MSC_EPOUT_ADDR 0x02
#define CUSTOM_HID_EPIN_NUM 0x01
#define CUSTOM_HID_EPIN_ADDR 0x81
#define CUSTOM_HID_EPIN_SIZE 0x02
#define CUSTOM_HID_EPOUT_NUM 0x01
#define CUSTOM_HID_EPOUT_ADDR 0x01
#define CUSTOM_HID_EPOUT_SIZE 0x02
Descriptors are as follows:
Device descriptor:
0x12, /*bLength */
USB_DESC_TYPE_DEVICE, /*bDescriptorType*/
0x02,
0x00, /*bDeviceClass*/
0x00, /*bDeviceSubClass*/
0x00, /*bDeviceProtocol*/
USB_MAX_EP0_SIZE, /*bMaxPacketSize*/
LOBYTE(USBD_VID), /*idVendor*/
HIBYTE(USBD_VID), /*idVendor*/
LOBYTE(USBD_PID_FS), /*idProduct*/
HIBYTE(USBD_PID_FS), /*idProduct*/
0x00, /*bcdDevice rel. 2.00*/
0x02,
USBD_IDX_MFC_STR, /*Index of manufacturer string*/
USBD_IDX_PRODUCT_STR, /*Index of product string*/
USBD_IDX_SERIAL_STR, /*Index of serial number string*/
USBD_MAX_NUM_CONFIGURATION /*bNumConfigurations*/
Configuration descriptor:
0x09, /* bLength: Configuation Descriptor size */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType: Configuration */
LOBYTE(USB_MSC_CUSTOMHID_CONFIG_DESC_SIZ), /* wTotalLength in byte */
HIBYTE(USB_MSC_CUSTOMHID_CONFIG_DESC_SIZ),
USB_MSC_CUSTOMHID_INTERFACE_NBR, /* bNumInterfaces: 2 interface */
0x01, /* bConfigurationValue: */
0x04, /* iConfiguration: */
0xC0, /* bmAttributes: */
0x32, /* MaxPower 100 mA */
Is there anything missing or wrong in descriptors?
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.