STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 ADC1 DMA Works while ADC3 DMA does nothing

So I have two channels configured basically with same settings. ADC1 works fine and DMA gets triggered and handled well. ADC3 DMA refuses to trigger any interrupt (not even an Error). The only difference is that ADC1 handles 14 channels while ADC3 ha...

Duddie by Associate II
  • 1989 Views
  • 3 replies
  • 0 kudos

Hello guys, I am on project that requires over the air firmware update Is there any guide+firmware for this task (eg from CUBEMX)?

I am using Nucleo-f446re and communicate with a server trought a GPRS telematic device ( the communication with the telematic device is through uart protocol). My average firmware size is 35kB. I can safely transmit the hex file to the MCU but I ne...

stathpale by Associate II
  • 3677 Views
  • 7 replies
  • 0 kudos

CMSIS DSP arm_rfft_q15 troubleshooting

Hello I am trying to perform FFT on real data sampled with ADC However, first I need to perform it on test data that I generated inside my code to verify it would workI set parameters: frequency, buffer size, sampling rate (buffsize 512)then I gener...

hashtala by Associate II
  • 1817 Views
  • 0 replies
  • 0 kudos

f_open not working in stm32f4 with FATFS

I'm using STM32F4 Discovery board and its expansion board for SD-card interfacing. I'm using SD-cards with DMA2 and STM32CUBEIDE FW_F4 V1.24.2Before pointing out error I want to attach below link as a reference which I've used in my code -https://co...

0693W000002lhz4QAA.png
Rsrma.1 by Associate III
  • 1222 Views
  • 0 replies
  • 0 kudos

Resolved! Custom Bootloader STM32H750

Hello,I am developing a simple GUI for a custom board based STM32H750 MCU.My requirements are the following:Both application code/data and touchGFX images/fonts are stored in and external QSPI (0x90000000) The entire application must be executed in t...

PLago.2 by Associate II
  • 1906 Views
  • 1 replies
  • 0 kudos

Connect to MQTT Broker with STM32F746G Discovery

Hi, I'm trying to connect to my MQTT Broker with STM32F7 Discovery kit.Firstly, I used MQTT Client in LwIP stack. When I call this function: mqtt_client_connect()the Error return ERR_RTE, mean Routing Error /** Routing problem.     */ ERR_RTE    = -4...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.