2024-10-18 4:55 AM
How can I achieve optimal range for LoRa node-to-node communication? I'm using the RFM95 module at a frequency of 932 MHz but experiencing very poor range—data transmission cuts out at only 4 feet. I have a compatible antenna, which is properly soldered as well.
Solved! Go to Solution.
2024-10-18 5:10 AM
I don't think so. And even if it is, is not something that ST delivered. So, you need to check with the person who worked on this FW.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-18 5:02 AM
Hello @Zeeshan123
This depend on the module you are using for LoRa communication (the RFM95 module). So, it will be a good idea to check with the manufacturer of this module. The 4 feet to me seems to be very strange for me.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-18 5:08 AM
Yes, its strange for me as well. I dont what might be the issue probably the module is the bad or the firmware needs revisions
2024-10-18 5:10 AM
I don't think so. And even if it is, is not something that ST delivered. So, you need to check with the person who worked on this FW.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-18 5:13 AM
I have downloaded the library provided by ST. I guess there might be bad chip or some hardware issues
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.